EEO#.MODE
Description
This keyword specifies the type of output waveform an EEO generator will create.
SOURCE | ||
---|---|---|
0 (default) | A Quad B |
![]() |
1 | CW/CCW |
![]() |
2 | Step/Direction |
![]() |
Examples
Code
This will set the 2nd EEO output mode to Clockwise/Counter-clockwise.
-->EEO2.MODE 1
Context
For more information see Output - Encoder Emulation.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 0 to 2 |
Default Value | 0 |
Data Type | Integer |
See Also | |
Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.